This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22810: Load Switch recommendation

Part Number: TPS22810

Do we have A load switch, input 4V, output RMS current 1.5A, maximum transient current 2.3A; The operating static current is required to be less than 50uA, the internal resistance is required to be less than 50mohm, and most importantly, reverse protection in the ON state.

  • Hello Xiaofu,

    The only device we have that has always-on reverse current protection that fits the criteria you've listed is TPS22950; however, Its Iq MAX is 60 uA (40 uA typ). All other options with always-on reverse current protection has a higher Ron that what you've listed. 

    Regards,

    Kalin Burnside