This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61165: 2 LED STRIPS -400mA @ 12VDC EACH

Part Number: TPS61165


Hi Team,

We are going to design a circuit with an input of 12VDC that consists of 2 LED strips running simultaneously which should have 400mA @ 12VDC individually along with PWM dimming control. For this application, we are going to use "TPS61165" Driver IC. With the help of the application circuit in the datasheet, we have designed the preliminary circuit. Please verify the circuit and give us your comments on whether this design can meet our specifications (Check discrete components values as well which should meet our output requirement).

Below you can find the attached design.

Reference Circuit