I am seeing a fault in the status register when we have a low input voltage on the charger input. Please note that this voltage is not so low as to trip the undervoltage state. When I look at the fault register there are no faults, which per the datasheet would indicate an ILIM fault. However, I have monitored the current with an ammeter and a scope w/ current sense resistor and am not seeing any current value that would trip ILIM (400mA)
I am suspect to the fact that the input voltage at which the fault occurs is dependent on the SOC of the battery. Further, it seems to correlate with the Vsleep threshold. For example, if I have a battery 3.706V, the definition of Vsleep dictates that it would enter the sleep state between a VIN 3.771 and 3.826. The fault occurred at a VIN of 3.78V.
My suspicion is that we are entering this Vslp state. I am curious as to whether entering Vslp would result in a fault in the charger status register