This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8866-Q1: CPUMP current

Part Number: LP8866-Q1


Hi All,


I have a question about the CPUMP pin of the LP8866-Q1.


(1) Please tell me the theoretical value of the current of the CPUMP pin.
(2) Please also tell us about the theoretical value of the inrush current when the voltage of the CPUMP pin rises.

<conditions>
VIN 26V
VDD 3.3V
Ccpump 4.7uF (Conect to CPUMP pin)
SW Freq. 500kHz

Best Regards,
Ishiwata