This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2776: Vout drop when start up at -40°C

Part Number: LM2776


Hi team,

my customer are using LM2776 in series to have -10.6V output voltage, the schematic is below.

Phenomenon: when start up at low temp(10℃~-40℃), the second stage only reach -7, can't reach -10.6V. if start up at room temp or start up at room temp and then decrease temp to  -40℃, it won't have this problem.

Q:

1. what would possible cause this?

2. I read some of the thread, it seems LM2776 has known problem during start up, is this correct?