This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR36520: Maximum value of current

Part Number: LMR36520


Hi team,

In synchronous rectification, the peak currents flowing through the two MOSFETs are equal, which is the maximum value of the inductor current.

The current tolerance of the lower tube is smaller than that of the upper tube.

Does this mean that although the top tube current can reach 2.4A, it cannot exceed 1.8A in practice?

In practical applications, the current of the down tube can not exceed 1.8A or not exceed 2.3A or 2.8A?Thanks.

Best Regards

Charlie Xiao