Hi,
I would like to use a small solar cell to charge a single NiMH battery (between 500 and 1000mAh). The solar cell's ouptut is about 1.5V, so I'd probably use 2/3 of them and boost the output to a regulated 5V. The end-product will be used to recharge batteries while on outdoor hiking trips, meaning that the solar cells will be mounted on top of the hiking bags.
I've considered the bq2004, but would prefer not to have an external constant current regulator. Are there any chipsets in the TI portfolio that does not require external current sources? I suspect not, so I'll continue with the asumption that I'm going to use a bq2004.
1) If I walk under a tree and the solar voltage drop, what would the effects be, assuming that the battery has been charging for some time by then. I.e. the input voltage will be zero, and the battery voltage will be higher.
2) For batteries from different manufacturers, ranging from 500mAh to 1000mAh, will a C value of 1 be acceptable?
3) In order to keep the solution cheap and easy, I would prefer to skip temperature sensing. Can I simply connect TS to ground?
Finally, if I'm asking stupid questions and you know of a resource that will save you time by my reading it, please post a link? I'll gladly read up on the subject, on which I'm less informed than I'd like to be, rather than wasting your time by asking basics all the time.