Hi,
This is Regarding MPN - TPS54160DGQR
My Requirement is - 6-36V - Input, 5V & 1A - Output, Ambient - 85degC & Switching Frequency - 450-550KHz
Can you Please Provide me the following data for above Requirements:
1. High Side MOSFET Drain to Source ON resistance
2. Low Side MOSFET Drain to Source ON resistance
3. High side MOSFET gate charge.
4. Low side MOSFET gate charge.
5. Regulated Internal Voltage generated by BUCK IC.
6. External Supply input to internal regulator of BUCK IC.
7. Rise time of BUCK IC internal mosfet
8. Fall time of Buck IC internal Mosfet.
Regards,
Ajay