Hello,
We were trying to debug the issue with our charging circuit not functioning. Our charging circuit is shown below. We have two boards that have have a non functioning charging. There was no indication of short in the Vcharger PIN to GND and VBAT PIN to GND and the charger circuit was functional and was used a number of times prior. There is no output on the charger. when battery and 12V Power Adapter is plugged in. One board (BOARD A) shows STAT1 LED blinking when the 12V Adapter is plugged in while the other board (BOARD B) has no LED Turned ON.
After measuring the resistances of ICs pin to GND, we found the TS pin with RC14 and RC15 still connected to it, to measure around 40-50ohms on Both BOARD A and BOARD B. Board B also had VTSB read low resistance of 23ohm with respect to GND pin. We then removed RC14, RC15 and CC4 to check if the short was with the external components or with the IC.
The LOW Resistance measurements were still present
Summary of Resistance Readings
BOARD A
TS to GND: 54ohm
VTSB to GND: 30kohm
BOARD B
TS to GND: 43.4ohm
VTSB to GND: 23ohms
We would like to know what might have caused this issue. Is there any thing in our schematic that would have caused it? We have a couple more boards the have the same schematic and layout and we have been using them as well but they did not show this issue.
Prior to the pins shorting internally. with the resistors still on the PCBA, we were measuring near 20kohms at the VTSB pin and near 10kohms at the TS pin.
We look forward to your response.
Thanks,
Deniel