Other Parts Discussed in Thread: LM5021
Hey TI,
I was building a offline LED driver with input : universal (85Vac - 264 Vac) , Output : 20V @ 1.2A , with a DCM flyback
Wanted to use the UCC28740 as the control IC. The main aim was to maximize the efficiency for my design, for which I wanted to operate the IC at a Fsw lower than 100Khz - went thru the datasheet thoroughly , but it just mentions to operate with required fsw at maximum power.
My question is, is there a way to set the set the switching frequency externally thru some resistor setting?
Any reference or link would really be helpful,
Thank you!!
Rajat