Part Number: LM5156-Q1
Other Parts Discussed in Thread: LM5155-Q1, LM5158, LM5157, LM3481, LM5155, LM5156
Hi Team,
For the part number LM5156QDSSRQ1 below things are missing in the datasheet. Please reply to below queries ASAP.
1. Overload and short circuit circuit current limit value. Is it possible to configure the values of overload and short circuit current limit ?
2. Is it possible to run this regulator in BOOST mode without using external MOSFETs ?
3. Inside the datasheet its mentioned like regulator is having internal softstart ? Can you share the value of softstart time ?
4. Whether this part will support continuous/discontinuous mode of operation. If possible Application circuit for the same.
5. Is it possible to share the emission report for this component to check about the EMC aspects ?
6. Advantage/disadvantages of LM5156-Q1 compared with LM5155-Q1. While checking the datasheet I observed the below things. Please add if anything missing below
Advantages of LM5156-Q1 - Spread spectrum support, Higher Input voltage range.
Disadvantages of LM5156-Q1 - Non-availability of short circuit protection
Regards,
Siburaj D.S.