Other Parts Discussed in Thread: GPCRB
Hello,
During the discharge process, the PassedCharge() of the battery jumps, why is this? We recorded the value of CONTROL_STATUS synchronously, and found that CONTROL_STATUS also changed when jumping.
How can we avoid this problem? We have customized the chem id for the fuel gauge and optimized it with GPCRB. This leads to a jump in the SOC(from 14% to 0). How to solve this problem?
When configuring the fuel gauge, the current is reduced by a factor of two. So when recording the data, we doubled the signal of I, PCHG,TRC&TFCC. So the range of these signals is different with others.In addition, we found that under the current load conditions in Figure 1, PCHG jump is inevitable.
6813.002U放电前.gg.csv2工况放电-新测试柜1.0.3第2轮放电.xlsx
Sincerely,
Xiulan