Hello,
Can you tell me if there is another circuit, or another method to achieve the function shown in figure 7-4 of the datasheet (Supplement State Circuit) but with an input voltage of 11V to 17V.
In short, my problem to solve is that I use a module that I cannot touch (you have to see it as a black box). When this module start causes a current peak that my power supply is not able to provide. I can't change my power supply either. So I thought I was looking to solve this problem by "intercalate" a circuitry managing the charging and discharging of a supercap that could give a boost during start-up? (What the TPS61094 does if I understand correctly but not with the good voltage for me...)
For information my nominal input voltage is 15V but can vary between 11V and 17V. The maximum current of this power supply is 2A5. I need an extra 2A5 to be able to absorb this spike. The output voltage does not need to be specially regulated.
If you have another idea I'm a taker too ;-)
Best regards
Olivier