This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8312 ignoring reset signal



We are trying to use the DRV8312DDW driver in a design where we need to control the three half bridges separately. Only one of the half bridges is used as a switching node (A) with the other two (B and C) high, low or reset (with adjustments for avoiding BST_UVP when high). The problem is that half bridge B is always active (low/high depending on PWM_B), regardless of the level present at the /RESET_B pin. Half bridge C however works as expected.