Other Parts Discussed in Thread: BQSTUDIO
Hi Team,
The customer provides some devices that cannot communicate after OTP programming. The I2C waveform is shown below.
It can be seen that a NACK respond next to the address 0x10.
I exchange the device to our EVM. The result is red LED D3 turning on. According to the EVM Users' Guide, I think the FUSE or protector BQ771807DPJR are working. Also, the device cannot communicate with BQstudio on our EVM after exchanging.
I checked that various permanent fail(PF) will make the FUSE pin drive high, and it should be noticed that the Protection Configuration[PF_FUSEE] is disable in OPT programming according to customer.
Could you please give me some ideas to further debug this problem? In particular, please consider the situation that the secondary protection is working and communication with no ack. Thanks.
Best Regards
Francis Jiang