This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: FUSE terminals when using two BQ76952s

Part Number: BQ76952
Other Parts Discussed in Thread: , BQ7718

Could you tell me how to connect the FUSE terminals when using two BQ76952s?

  • Hi Kentaro,

    If the FUSE pins are not used, they can be left floating or they can be connected to a resistor to the VSS pin of each IC. If these pins need to control a fuse on the board, the BQ76952EVM shows how a fuse can be controlled with multiple stacked devices - there are 4 BQ7718 devices that are stacked to control one fuse. This same circuit idea can be used for the stacked BQ76952 FUSE pins.

    Best regards,

    Matt