Hi
I design with BQ4050 and use 4 LEDs, LED CHG THRESH1 is 0%,CHG THRESH2 is 25%,CHG THRESH3 is 50%,CHG THRESH4 is 75%,CHG THRESH5 is 100%.
The LEDs display is normal during the charging test. When the RSOC reaches 100%, LED2 and LED4 will flash, LED1 and LED3 are always on and normal. There is no such problem when testing with 5 LED lights.
I didn't set the LEDPF bit, only set the LDECHG bit.
How to turn off the LED2 and LED4 blink issue?
Thanks
Star