Hi
Please help and advise? RESET IC can do the following timing control
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gareth,
Thank you for your question, I will be happy to help. For the TPS3899, the sense delay can be setup to ignore fault pulses smaller than than the sense delay time up to 6.2 seconds, 10μF on CTS pin. Similarly the reset time delay can also be adjusted with a capacitor on CTR, up to 6.2 seconds, with 10μF on CTR.
Based on the TPS3899 capabilities it is able to perform your timing diagram.
Jesse
Hi Gareth,
Which one do you need longer than 6.2s the Sense delay or the Reset delay?
Jesse