Other Parts Discussed in Thread: BQ25792, BQ24196,
Hello,
I have a PD (TPS25750D) trying to power a flash drive when its in DFP mode. For some reason, the 5V on the VBUS pins are toggling the 5V on and off continuously. Our 5V supply on the PP5V pins are stable. This only appears on the other side of the internal FET.
Our settings in the GUI binary file were:
15W
15W
Power Source
device
USB2
Not sure why it is doing this. Need help troubleshooting this issue. The PD does not detect the flash drive at all. The 5V toggles with or without the flash drive plugged in.