Other Parts Discussed in Thread: LP3907
Hi Team, seeking some assistance.
The following is an article about SW1, SW2 OPERATION that can be found on page 20 of the data sheet for the part.
"The default output voltage for each buck converter is factory programmable."
1. Does this article mean that the default output voltage can be programmed by the customer at the factory?
2. I have confirmed that PWM mode can be forced the PWM mode through the setting of the buck control register.
But is it possible to set the PWM mode through factory programming without accessing the register?
3. It was confirmed that a 13MHz clock should be input to the SYNC pin when using the external clock synchronization function.
But, in our system, it is difficult to generate a synchronized clock of 13MHz.
If I input the 12.288MHz clock or a clock of a different frequency to the SYNC pin as an external clock, is there any problem in operation?
Thank you
-Mark