hi there
I have a customer who is using BQ24707 but they are worried about the over charging of the battery.
below is a situation that customer have mentioned:
For example : Require to charge a 4.2V battery. But the wrong setting of charge voltage is 12V. The 4.2V battery will be over charge. Although most of the battery has the overcharge protection and cut off the charging at around 4.4V, this does not 100% safe for the protection circuit of the battery will not fail.
Battery is a 1 ~ 4 cell battery and max charging current is @ 4A.
Any recommendations?
Thank you!
Adam