We are evaluating using TPS23841, however we do have a CPU on board that we would like to use to manage the 23841.
Is there a firmware we can port to run on our CPU or is the firmware only available if one use's the TI MSP430.
Either case where is the firmware and the documentaion so we can understand and evaluate the effort involved.
thank you