Hallo,
i use for a battery application the tps54060, the input is aprox 40V and the output taken 10V. However, i measure on the PWRGD pin the value that i have on the output. In this point i have to inform you that i do not have any osci. If someone have some idea what i make wrong , i would be thakful for a replay,
thank you6406.tps54060 42V -- 10V.pdf