We would like to use the BQ24075 DPPM charger ic which is in our design
To control charging temperature. we had been using the BQ27500.
All we need to do is connect a thermister to the TS line of the BQ24075
And this should work. However, it is not working right it seems.
The thermister kicks in and the charging is stopped while hot, but the charging
Will not resume once the temperature returns to in range.
We are on a very tight schedule with implementing this change and could really use
Some help. It may be a very simple issue that we just are not aware of yet.
-Tom-