Hi, I'm having problems with a bq24610. When I have a load connected on VSYS and no battery on VBAT, the board runs as expected and draws about 2.1A from the power supply. But as soon as I connect a battery with the VSYS load still connected, the power supply current draw drops to 1A. The power supply can supply 5.2A max. LEDs powered by VREF turn off so I think VREF drops (I've seen this happen before). I also have LEDs indicating STAT1 and STAT2 and these both turn off. I also see the battery voltage begin to drop. This sounds like the bq24610 is not switching correctly and it is drawing power from the battery instead of the power supply. Does anyone know what could be wrong?
Thanks,
Ron