Can TPS61165 configuration as buck-boost? we are considering this to drive LED.
Thanks,
NT
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The term "buck-boost" originally referred to a converter that took a positive voltage and converted it to a negative voltage. Now, the term refers to a converter that provides an output voltage from an input voltage range that can be higher and lower than the output voltage. There are four switch, single inductor converters (e.g. TPS63000) that change from being a buck converter if Vin>Vout to a boost converter if Vin<Vout. A boost converter or boost converter based WLED driver (e.g. TPS61165) can be configured as a SEPIC converter, with two inductors and additional capacitor (instead one inductor in a boost configuration) in order to provide an output voltage that is in between the input voltage range.