This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq20z95 stuck with no communication please help

hello

i have 2 question:

1. i am trying to load GG file into the battery pack

i followed the istruction in the "Using bqTester single site software"

in section 4 - creating golden image, i programmed the SENC file , then sent 08 word to ther SMBus . now i cannot read or write to the device , also in SBS screen i cannot see communication.

2. the unlock code (default) is not unlocking the program. is there other code?

thank you

Roi Ofer