Hi,
We've created a board with OMAP 3530 (3730 in next revision) processor and the TPS65930 chip. We use WinCE 6.0 (we plan to move to 7.0), and all the drivers in BSP is prepared for TPS6550. They should be compatible, but we have some problems there - we cannot hear any sound. We are still working on it, and we'd like to eliminate as many potential issues as possible. Now, here is my question: Are there any differences between TPS65950 and TPS65930 in terms of driving audio? Should the TPS65930 chip work with all the settings from TPS65950 or there are some changes needed in BSP?
Please, let me know.
Thanks a lot!
Zack