The TPS62420 Eval Board uses isolated top copper only connections for the input and two outputs. The input voltage and associated grounds are all separate traces. However, in the real world the input and two output grounds must be all be connected. I'm using a 4 layer PCB and interconnections for the TPS62420 are on layer 3, while layers 2 and 4 are solid copper (layer 1 is top copper and components). Because of noise issues I'm using MuRata 1uF feed-through capacitors on the input and both outputs. So at this point the ground planes and top copper grounds will all be connected together.
Even with shielded inductors I've noticed that radiation is quite bad. So I've laid out for a Laird board level shield over the entire switcher. This also makes it hard to isolate grounds as the shield connects all grounds around the switcher.
My first thought was to run keep outs on the inner layers to control where the ground currents flow. Now I'm wondering if I'm over thinking this and should simply allow the inner ground planes to connect all grounds internally and simply follow the eval board layout to control ground currents in the immediate vicinity of the switcher. Another thought was that if I used keep outs to control the ground currents, to arrange them so as to create an internal star ground system where all grounds connect at a single point where they attach to the internal ground planes.
Any advice, especially from experience would be welcomed.