This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62824A: Ball composition

Part Number: TPS62824A


Our customer ask us the following question to register the device in which Sn is used, and could you kindly tell us the detail?

Material: TPS62824ADMQR

1. Use Ni for grounding or not. : Yes / No

2. Thickness of outermost layer plating : 10 μm or more / Less than 10 μm

3. Heat treatment such as annealing or not : Yes / No

Your prompt support would be highly appreciated, thank you!