Hi
I saw the typical application from datasheet of UCC2808AD-2,so can anyone help to explain below:
Q1: what is ① used for ?
Q2:why add an inductor connected to GND as noted with ② ?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I saw the typical application from datasheet of UCC2808AD-2,so can anyone help to explain below:
Q1: what is ① used for ?
Q2:why add an inductor connected to GND as noted with ② ?
thanks
Hi Xi,
(1) This is a full-wave rectifier. It charges the 10uF capacitor on the VDD pin if either OUTA or OUTB is ON. If a single diode were used then only OUTA (or OUTB) would charge the 10uF capacitor.
(2) The inductor works with the output capacitors to form an LC filter. Usually the inductor is drawn as shown below, but it could be placed in either location with the same effect.
Regards,
Eric