This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dual Output power supply low component count

Other Parts Discussed in Thread: LM5143, LMR38010, LM5145

Hi Team,

We need a dual output non-isolated converter . Specifications are as follows, 

Input : 40V to 70V , 

Output1 : 24V / 6A limited,

Output2 : 12V / 1A limited 

Operating Temp : 0-40C

Can you please specify a suitable controller /Regulator with low component count ?

Thanks,

Sivamani

  • Hi Sivamani,

    We have a dual-output controller - the LM5143 - but it's rated to 65V operating, 70V abs max.

    12V/1A is ideal with a converter (integrated FETs). Consider the LMR38010 80V/1A converter (also available in 2A). 

    24V/6A requires a controller - take a look at apps example #3 in the LM5145 datasheet.

    Note, SYNCOUT of the LM5145 may be able to drive SYNCIN of the LMR38010, thus achieving some input ripple current cancellation.

    Regards,

    Tim