Hi:
We are using BQ34Z100-G1, and after the Full Sleep mode enabled to save power, we noticed that the IC communication will get interrupted (all registers are 1) every 10 seconds, which is consistent with the FS wait time. Before FS was set, the I2C communication was good.
Test conditions:
No current flow, I2C pulled up, I2C communication every 400ms, I2C rate 100kbps.
In BQ34Z100-G1 spec, it stated "The gauge exits the FULL SLEEP mode when there is any communication activity", but if the communication exists, will the IC falls into FS mode? And wake up immediately because of communication? And this FS caused the I2C interrupted?
Thank you!
Chen