Hello,
My customer considers using the TPS568230 with the following conditions.
- VIN=12V, VOUT=2.5V~5.5V, FSW=1MHz
1. Are there any problems using the above conditions?
Is there any limit on the VIN input range depending on the FSW setting?
2. Are there any recommended operation modes under the above conditions?
Which of the three operation modes is the most advantageous?
Thank you.
JH