This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EV2400: Connection issue

Part Number: EV2400
Other Parts Discussed in Thread: BQSTUDIO,

I have got a EV2400 and connected it to the battery pack, downloaded the latest BQstudio and got FW updated. But the USB was not present and the I2C has not response. Would you be able to help?

  • Hello Rong,

    If you were able to update the firmware, then the hardware is communicating on USB. Check if another instance of bqStudio is running or if another program is using the EV2400. If you are not sure, then reboot the PC and check.