Hi,
Good Day. I have a customer who is working with LMG1020. Please see below the query of our customer for your reference. Thank you very much.
I want to ask a question about LMG1020.
Based on data sheet, it can burst gate of n-channel MOSFET with 1A to 5A.
Is there any minimum power input requirement for this IC?
For example, for 1A charge current, it is ok to use 1W isolated dc-dc module (12V to 5V)?
Based on my system requirements, I am designing isolated MOSFET gate driver. For this, I have plans to use LMG1020.
For LMG1020, is there any power requirements for VDD?
I am planning to drive DMG2302UKQ-7 with 1 or 2A gate current.
For this, is it okay to use 5V 0.2A power source?
Based on your EVM, they used 0.1A LDO to drive this IC.
Best Regards,
Ray Vincent