Other Parts Discussed in Thread: TPS23731, , TPS23734
Hi
We are designing a product that will be connected over Ethernet throguh an RJ45 connector and be powered over Ethernet with PoE+ class 4. We are looking at ICs for power negotiating and from what I can read up on the Internet it seems like its two ways to negotiate PoE+, type, class 4 power = 30W.
Eiher HARDWARE BASED or SOFTWARE BASED/LLDP.
And from what I can read up it seems like the 802.at standard specifies that PoE+ PSE equimpment has to at least implemnt one of them, but PoE+ PD equipment has to implement both.
Based on this it seems like like if we are going to be compliant with 802.at standard, as a PD equipment we have to implement both, but almost all IC we have looked at for power negotiating only supports HARDWARE based negotating.
Does this mean that PoE+, class 4 power negotating is almost always done with HARDWARE BASED negotiating, and that LLDP is very uncommon and unlikely to experience for typical PSE equipment?
Anyt reccomendation for PoE+ ICs to use would be appreciated