We are making use of both EN1 and EN2 pins in Dual Output mode configuration for generating 1.8V/6A and 1.5V/6A.
EN1: Pull-up is Vin(12V) with Rent = 100k and Renb = 10k. 1.8V is fed to this pin
EN2: Pull-up is 5V with Rent = 100k and Renb = 10k. 1.5V is fed to this pin.
Switching Frequency : 1500kHz
Is there any fault in the above values ?