Other Parts Discussed in Thread: BQ40Z50-R2,
Hi engineers,
I found that BQ40Z50-R2 added DSG_ 0_ SMOOTH_ OK. In addition, the parameter settings related to smooth have been added in gasguaging, According to this DSG_ 0_ SMOOTH_ Understanding of OK definition, this bit will start to smooth within a certain voltage range at the discharge end to avoid jumping to 0%;
The question is: 1. The original smooth function does not include DSG_ 0_ SMOOTH_ OK function? 2. No DSG_ 0_ SMOOTH_ OK in BQ40Z50-R1, does it mean that the RSOC at the discharge end may jump to 0?
Sincerely