This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM5D1806: Schematic Review

Part Number: TPSM5D1806

1806.pdf

For generating 1.8V and 1.5V output voltages, we are forcing the respective voltages in the Enable pin as shown in the pdf. Is it the correct way to do and what will be the voltage level in EN1 and EN2 pin respectively?

  • Hello Karthik, 

    I re assigned this to Ryan Chen, we will provide review next week 

    Thanks!

    Tahar

  • Hi Karthik,

    The way to adjust the output voltage is to change the feedback resistor divider which is placed at the output instead of at EN. 

    The device will work when EN is greater than 1.2 V and stops switching when it falls below 1.1 V. 

    In your case, for 1.8 V output, I would recommend the top feedback resistor of 26.1k and the bottom feedback resistor of 10k.

    1.5 V output I would recommend the top feedback resistor to be 20 k and the bottom feedback to 10 k. 

    Best, 

    Ryan