Hi,
I have questions about the Cff cap for LMR51430YFDDCR (1.1MHz Forced PWM). I don't see any mention of it on the datasheet. This cap showed up when I used Webench to design the following configurations:
- 3.3V @ 0.4A (1.24A doesn't seem to require Cff cap)
- 1.5V @ 0.57A
How is the value calculated and at what current is the cap required? We are interested in using the same value cap for both the 3.3V and 1.5V rail. Is this possible? If so, would 47pF work for both or is there a better value?
Thank you