This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTN78020W: relation between free-air temperature and aging test temperature

Part Number: PTN78020W


Dear team,

I get a problem:

First party requires us to do aging test with 65℃/24h. We have a PTN78020W on the board and it increase to 67℃ when room temperature is 27-28℃.

In this case, when room temperature is 65℃, the PTN78020W will reach 105℃, which is over 85℃ ABSOLUTE MAXIMUM RATINGS in datasheet.

Specally, the PTN78020W is a multi-chip device without a Jc parameter, so I do not know how to check the device can be aging test in 65℃/24h or not.

Best regards,

HuangFeng