Other Parts Discussed in Thread: TIDA-010000
Hello,
I am using the UCC28740 flyback controller for stepping down the Input voltage. For this design, the Input voltage range is 200-800 V dc and it has multiple output voltages. One of the outputs(18V) is being regulated.
Currently, the output voltage is not rising more than 5V for 24V output and 3.5V for auxiliary winding which is connected to VDD (nominal voltage 12V).
We have checked the VS and CS pin waveforms and by the look of those, it does not seem that IC is going in OCP or OVP mode. However, The VDD Voltage is oscillating between 21V and 7.5V suggesting IC is restarting.
What might be the reason behind this as all components are already according to design calculations following the design guide for TIDA-010000. Maximum Switching frequency is 36kHz.
I suspect the due to low output voltage , FB pin current IFB is also low so VCL voltage will be high and controller will try to switch at higher frequency but maximum frequency is limited to 36kHz in this specific design. Please help regarding the issue of low output voltage.
Quick help would be appreciated.
Thanks,
Jasvant Singh