This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21540: DW can use DWK to replace

Part Number: UCC21540

Hi expert,

My customer is choosing dual channel isolated gate driver.

and if they are fine with UCC21540DW specs and they can also just use DWK package to replace. Am I right?

since they care about the supply and they want to confirm it.

BR

Emma

  • Hi Emma,

    Thanks for using E2E! Yes the DWK and DW are the exact same device. The only device is the NC pins in between the ChA and ChB are removed for DWK. This helps to increase cross channel isolation for the DWK package.

    Regards,

    Akshat