Other Parts Discussed in Thread: BQ24075
Dear TI
I am circuit shown in attachment but issue is that BQ25070 was not able to start properly on battery. it's output fluctuate and drop to approx 0.15V and keep fluctuate at the frequency of 2Hz approx. If the Input (USB 5V) is connected ot works fine and but not able start on the battery (li-ion 3.7V-4.1V). One it remain stable if the charger connects and removed back. it charging the battery as will only causing the issue when system start from the battery. Even the battery is fully charged.