Hello everyone,
I'm finding some issue on using BQ2000 while trying to charge 2 batteries Ni-Mh.
I started with the suggested schematics here below (pag.10 of the datasheet).
The only difference I use N-MOS instead of BJT for Q1, Q2 and Q3 and I added
a pull-up resistor.
I don't use any thermistor so I changed R4 and R5 in order to be in the working range.
I made some test with 3 batteries and the circuit works fine.
I supposed to just change the ratio between R6 and R7 (the divider for the battery voltage)
in order to have the same voltage on pin4 (BATT).
Unfortunately that doesn't seem to work. The RC pin doesn't start to work with the expected
sawtooth signal, the LED pulse around 1Hz without starting the charge.
It's like the IC is in charge qualification and doesn't proceed. But I don't see any
problem that should prevent the fast charge step.
I have measured:
Vcc=4,5V
VBAT=1,55V
VTS=1,85V
What I'm missing?