Hey team,
I'm doing a power project for my FAE rotation, and I'm brand new to Altium in which we will do a PCB design and layout. I see there are a ton of options in the Manufacturer Part Search, but only a couple that I'm able to download. I was wondering if there was a downloadable PN that your team suggests that is footprint-conscious (and has good availability, as I'm sure that's a worthy parameter in this project simulation).
Also feel free to stop me where I am and point me to a different direction if there's other steps I need to take in Altium before preparing my board with these parts. It's part of a power tree that has a 3.3V to 1.8V 0.2A rail, keeping cost as a key careabout (but with concern of 3% undershoot/overshoot transient on 25% to/from 75% load)
Thanks in advance for the assistance!
Marco A Rojas