Part Number: LM5164
Other Parts Discussed in Thread: UCD3138, PMP4333, LM5177
Hi Experts,
Could I ask whether we have any solution or reference design can meet Vout (5-48V), Iout (Max 5A), Pout (240W max) ? Input can be either AC or DC. If we have any buck can meet, just make sure the buck Vin is greater than 50V. If we have any buck-boost, then the Vin range should be not that important.
Thanks!
Dylan