This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
KEEP UPDATING...
[Q1]: What are the main differences between LP5891-Q1 / LP5891 / LP5890 / TLC6984 / TLC6983?
[Q2]: How to quickly light up a LED panel with LP589x / TLC698x? Where is the sample code?
[Q3]: How to configure the color / brightness / color temperature?
[Q4]: How to implement CCSI? Is CCSI compatible with SPI?
[Q5]: How to select power supplies VR, VG, VB and VCC?
[Q6]: Could you provide more relevant resources for LP589x / TLC698x?
[Q1]: What are the main differences between LP5891-Q1 / LP5891 / LP5890 / TLC6984 / TLC6983?
From the functional point of view, the main differences between those devices are shown in Figure 1.
[Q2]: How to quickly light up a LED panel with LP589x / TLC698x? Where is the sample code?
An easier and quicker way is using the evaluation module (EVM). Here are the procedures (You can find the links in Table 1):
Table 1 Summary of Useful Links
Device |
Evaluation Module (EVM) |
EVM User’s Guide |
Sample Code |
Sample Code |
Registers Map |
Sample Code Support Items |
||
Frame rate control |
SCLK frequency control |
Diagnostics support |
||||||
LP5891-Q1 |
LP5891Q1EVM-SW-F280039C |
x |
x |
x |
||||
LP5891Q1EVM-SW-F280039C |
x |
x |
x | |||||
x |
x |
x | ||||||
TLC6984EVM-F280039C-SW |
x |
x |
x | |||||
TLC6983EVM-F280039C-SW |
x |
x |
x | |||||
LP5899DYYEVM | Download | LP5899DYYEVM-LP5891-F280039C-SW |
|
x |
x |
x | ||
LP5899DYYEVM-LP5890-F280039C-SW |
|
x |
x | x | ||||
[Q3]: How to configure the color / brightness / color temperature of the LED panel?
Table 2 shows the basic register settings that configure the brightness, color temperature and color. You can refer to Register Maps section in the datasheet.
[Q4]: How to implement CCSI? Is CCSI compatible with SPI?
[Q5]: How to select power supplies VR, VG, VB and VCC?
[Q6]: Could you provide more relevant resources for LP589x / TLC698x?
Other resources: