Other Parts Discussed in Thread: LM5022
Hi Team,
If the voltage at the current sense comparator input exceeds 0.5 V, the MOSFET gate drive is immediately terminated.
When will the MOSFET be turned on again? Thanks.
Regards, Charlie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Brigitte,
Thanks for your update.
When the CS point voltage reaches 0.5V and the current protection is activated, will the capacitor in the picture discharge immediately? Thanks.


Regards, Charlie
Hi Brigitte,
If the output terminal is short-circuited, can the current protection of the LM5022 not protect the secondary circuit? Thanks.
Regards, Charlie
Hi Brigitte,
Thanks for your update.
When customers are developing, LM5022 is used for non-isolated flyback. When the load is short-circuited, the current on the secondary side of the transformer becomes very large.
But I think that the current protection of LM5022 only limits the power of the circuit, there is no way to ensure the safety of the flyback's post-stage circuit, right? Thanks.
Best Regards,
Charlie Xiao